Part Number: RM48L950
Other Parts Discussed in Thread: HALCOGEN,
Hi Ti,
Our project should be complaint to IEC-61508, so we need to perform MCU inbuilt diagnostic periodically. The SafeTI diagnostic library provides the library driver to perform these diagnostics. I have some doubts that are related to SafeTI diag library, Halcogen and CCS.
i. SafeTI diagnostic library API will perform boot-time diagnostics at sys_startup.c file and periodic diagnostic at main.c file. Is my understanding correct?
ii. What is the purpose of configuring the SAFETY INIT tab in halcogen. Is it has any relation with SafeTI diagnostic library? Or it is mandatory to configure in Safety Init, if the SafeTI diagnostic library is used?

iii. Is it required to enable Group1 interrupt for the ESM module when SafeTI diagnostic library is used?
iv. Please provide the steps to integrate the safety diag library into a custom CCS project?
Regards,
Monish P