Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN
I did not see a HalCoGen E2E group, so hopefully this is the correct forum. In HalCoGen (04.07.01), in the TMS550LC4357ZWT tab and PLL page, the 2 divider-selection blocks for each PLL ("PLL 1 Div" and "PLL 2 Div") numeric selections don't change the PLLCTL registers. As I interpret the TRM, these 2 numeric selections ought to change these 2 lines of code:
systemREG1->PLLCTL1 = (uint32)0x80000000U
| (uint32)0x20000000U
| (uint32)((uint32)0x1FU << 24U)
and
systemREG2->PLLCTL3 = (uint32)((uint32)(1U - 1U) << 29U)
| (uint32)((uint32)0x1FU << 24U)
Yet no matter what is selected in the PLL1Div and PLL2Div, the value shifted-up 24 is always 0x1F.
Please check on your HalCoGen.
Thanks,
Jim