Part Number: TM4C123FH6PM
Hello!
As a part of my design I need to create device wich uses CAN bus to connect to other devices and USB to connect to host. This device should add CDC device for each CAN device connected to, and remove it then disconnected.
As I read spmu297e document, I see the USBDCDCCompositeInit() function to add composite device, and USBDCDCTerm() for shuting down, but there are a note: "This function should not be called if the CDC device is part of a composite device and instead the USBDCompositeTerm() function should be called for the full composite device." But I do not need to shut down whole composite device, but only one CDC device, how to do it?
Thank you!