This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-EXP432P401R: Zephyr Hello World

Part Number: MSP-EXP432P401R

Hi, I am trying to get a working demo up for the Zephyr OS on you MSP432 Launchpad but having trouble. See attached for description, I get this error -

24 | #error "Unsupported board: led0 devicetree alias is not defined"
      |  ^~~~~
[5/112] Building C object zephyr/CMakeFiles/zephyr.dir/lib/os/dec.c.obj
ninja: build stopped: subcommand failed.
FATAL ERROR: command exited with status 1: /usr/bin/cmake --build /home/jmreina/zephyrproject/zephyr/build

Seems simple to fix but I am stuck, how do I get this blinky demo to run on my Launchpad? Thinking

@brief 		TI Zephyr Debug Notes
@details 	TI MSP-432P401R Launchpad
@auth 		Justin Reina
@date 		8/23/21


@section 	Procedure [2]
	Create a fresh VM of Ubuntu 20.04

	Update & Upgrade
		sudo apt install git gitk
		sudo apt update
		sudo apt upgrade

	Get Kitware
		wget https://apt.kitware.com/kitware-archive.sh 
		sudo bash kitware-archive.sh

	Use apt to install the required dependencies:
		sudo apt install --no-install-recommends git cmake ninja-build gperf \
		ccache dfu-util device-tree-compiler wget \
		python3-dev python3-pip python3-setuptools python3-tk python3-wheel xz-utils file \
		make gcc gcc-multilib g++-multilib libsdl2-dev

	Install west
		pip3 install --user -U west
		echo 'export PATH=~/.local/bin:"$PATH"' >> ~/.bashrc
		source ~/.bashrc

	Get the Zephyr source code:
		west init ~/zephyrproject
		cd ~/zephyrproject
		west update

	Export a Zephyr CMake package
		west zephyr-export

	Zephyr’s scripts:
		pip3 install --user -r ~/zephyrproject/zephyr/scripts/requirements.txt

	1. Download the latest SDK installer:
		cd ~
		wget https://github.com/zephyrproject-rtos/sdk-ng/releases/download/v0.13.0/zephyr-sdk-0.13.0-linux-x86_64-setup.run

	2. Run the installer, installing the SDK in ~/zephyr-sdk-0.13.0:
		chmod +x zephyr-sdk-0.13.0-linux-x86_64-setup.run
		./zephyr-sdk-0.13.0-linux-x86_64-setup.run -- -d ~/zephyr-sdk-0.13.0
		
		>src ctrl roots of zephyr-sdk-0.13.0\ & zephyrproject\

	3. Install udev rules, which allow you to flash most Zephyr boards as a regular user:
		sudo cp ~/zephyr-sdk-0.13.0/sysroots/x86_64-pokysdk-linux/usr/share/openocd/contrib/60-openocd.rules /etc/udev/rules.d
		sudo udevadm control --reload

	4. Build the Blinky Sample
		cd ~/zephyrproject/zephyr
		west build -p auto -b msp_exp432p401r_launchxl samples/basic/blinky

	Flash the Sample
		west flash

@section 	Notes
	@board 	TI MSP-432P401R Launchpad [1]
				*MSP-EXP432P401R
				*msp_exp432p410r_launchpad

@section 	Reference
	1. https://www.ti.com/tool/MSP-EXP432P401R
	2. https://docs.zephyrproject.org/latest/getting_started
Console Report.zip