Part Number: TM4C1294NCPDT
Hello,everyone!I think I'm in trouble, and I hope I can get your help.I've been studying radar tracking algorithms recently, referring to the TI documentation "Tracking_radar_targets_with_multiple_reflection_points.pdf" .The download link is Tracking_radar_targets_with_multiple_reflection_points.pdf.
At present, it is not clear to me how the radar algorithm parameter configuration will affect the radar recognition effect.For example, in Section 4.2.2 , if I change the value of setPointsThre from 5U to 1U, will I see multiple cars instead of one car?Is there a way to simulate the effect of radar algorithm parameter adjustment on radar identification?Like this