Part Number: MSP432E411Y-BGAEVM
Other Parts Discussed in Thread: MSP432E411Y
Hello Guys,
Good day.
Customer would like to know if MSP432E411Y can control TFT displays of 12.1" and 15" up to 1024 x 768 pixels and with full 24-bit colors?
Can the evaluation module handle necessary tests with such 15" displays? Which software tools can the customer use for fast screen implementation and tests?
Beyond LCD controller, they need Ethernet, USB, ADC, which MSP432E411Y already has. A 10-bit (or more) DAC with DMA to a RAM table would be a plus in case TI have another part number to offer?
Thanks and regards,
Art