Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN
Hi Support,
The MCU TMS570LC4357 generates CPU Interconnect global errors (ESM Group1, channel 52) that seem to be intermittent and random. Sometimes it takes up to 2 hours before to observe this behavior and some other times only few seconds after a power up.
The Interconnect status registers info are:
1. SDC Status Register = GLOBAL_ERROR bit set
2. Error Transaction ID Register = bit 4 set = Cortex-R5F CPU master.
3. Error Transaction Signature Register = bit 4 set = Cortex-R5F CPU master.
I know there is an silicon errata (DEVICE#49 False interconnect safety checker error flag) related to this kind of problems, but it does not help to solve the problem. The MPU is used and configured in a way that the entire memory from 0x0 to 0xFFFFFFFF is set to NORMAL, NOEXEC and then, the only memory that is configured as NORMAL and EXEC is the internal MCU flash memory from 0x0 to 0x003FFFFF. No other region is configured as NORMAL and EXEC. So far, the errata workaround is not working for us.
My questions are:
1. How to analyze deeper the root cause ?
2. How to know which memory access is causing the problem ?
3. How to know if it is a true or false interconnect issue ?
Regards,
Nicolas