Part Number: MSP432E401Y
Other Parts Discussed in Thread: UNIFLASH,
Hello,
I'm using a flash bootloader over UART on my MSP432E401Y, which I program via UniFlash.
It works fine when using the XDS110's UART, but not when using an external converter, such as an FTDI FT232.
After checking with an oscilloscope, I saw that UniFlash sends its first packet ([55][55]), MSP432E4 answers but UniFlash says it doesn't.
Then UniFlash should send the next packets as when working properly, but doesn't.
Is it possible to use UniFlash to upload code via UART using an external USB to UART converter ?
Thanks.
Regards,
Victor Tolosana