Part Number: TMS570LC4357
I am struggling to set up the PBIST Self Test. I am currently trying to run the PBIST Memory test for all RAM Groups as it is described in 9.6.2 Example 2 of the Reference Manual on Page 427. After running the test, the PBIST Registers are filled with:
RAMT = 0x02011208 -> (RGS = 2 , RDS = 1 ?)
FSFR0 = 1 (FSFR1 = 0 and all other Registers for Port 1 are 0 as well)
FSRC0 = 3
FSRA0 = 0
FSRDL0 = 0x0003765D
I am currently confused by FSRA0 being 0 as I would assume it to give me an Address in case of a failure and FSRDL0 as I do not fully understand what this Value is actually indicating or what it means?
For testing purposes I have tried to run the test on two boards but both of them give me the exact same result except for the FSRDL0 Register. FSRDL0 actually changed due to the change of boards and even on the same board it seems to be a little different every time the test is run.
So my question would be, what does FSRDL0 (FSRDL1) actually tell me and could I assume to have some flaws in my configuration as it seems to be a little odd that two boards indicate the exact same outcome except for the Failure Data and the Address being 0?