Part Number: TM4C129ENCPDT
Hello All,
I want to write program which can make software update by itself remotely. I did some research about that. THis can be done by seriport, ethernet, gsm,wifi.
what I understand is that there are some procedure or protocol.such as:
as a protocol it can be used ymodem.
But I guess we also need to write bootloader.
so I am confused abit. What is the right way to do this process.?
Do I have to write two program like one for bootloader and one for application?
Which surface is used most for software application remotely, gsm, wifi or something else? and also easy to implement? can you please advice and share some source/code/link for it?
How to implement ymodem protocol and where? in bootloader or application?
As you can see I have some question, if you have an answer for any of them, please let me know
thank you
Bekir
Best Regards