Part Number: MSP432E401Y
Other Parts Discussed in Thread: UNIFLASH
Hi,
I am trying to load a new application image via UART to the MSP342E401Y dev board, but without any success. I'm following all the steps outlined in this workshop MSP432E4 Bootloaders (ti.com)
- I have connected an Olimex BSL Rocket device to the BSL header on the board and bridged the two UART connectors on the dev board (R5 and R6) with zero Ohm resistors.
- I am using BSL Scripter v3.4.0.1 and looking at the E4xx_uart examples coming with it.
- When running the example script_1, I am getting one of two errors after the "Send the auto-baud sync bytes!" message when the scripts executes MODE E4XX COM18 UART 115200
- [ERROR_MESSAGE]No response bytes received from BSL! or (less often)
- [ERROR_MESSAGE]Initialization of E4xx BSL failed! Exit the scripter!
Do I need to change any other jumpers / connectors on the board? Should this just work with the ROM Bootloader?
I can update application images over Ethernet using BSL Scripter, but not over UART.
Same behaviour when using UniFlash:

Please advise.
Thanks, Steffen