Part Number: TMS570LS1224
How many SPI Ports are there in TMS570LS1224.
In Our design we have to connect following six devices over SPI
- x1 EEPROM
- x2 ISO SPI (LTC6820)
- x2 To connect external SPI based device
- x1 SD Card
1. Please suggest how to connect the above five devices
2. What maximus size of SD card and up to which SD Card Class we can connect over SPI. We are considering Class 10, 64GB SD card, will it work?
3. What is MibSPI and how it is different from Standard SPI. Can we connect the SPI based devices over MibSPI, and will it properly work?
Thanks!
Best Regards
Swadesh