This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS1114: could not burn in software

Part Number: TMS570LS1114

Dear ,

What can I do if the program fails to burn in after it burns normally in debug mode? Is there a Flash deadlock , and if so, how to resolve it? the error info as below,

[ERROR] CortexR4: Error connecting to the target: (Error -2062 @ 0x0) Unable to halt device. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.2.0.00002)

  • Hi Cooper,

    The problem might be caused by the code you have programmed. The code in the flash makes the CPU enter an exception state repeatedly, and the CPU is not able to enter a debug state.

    Please try this procedure to let CPU enter a debug state:

    1. Open the target configuration window, and launch the selected the configuration
    2. Switch to debug window.
    3. Press the reset (nRST) button and hold it.
    4. Click “Connect Target” immediately after you release the nRST button.
    5. The board should be connected after couple tries.