Part Number: TM4C1297NCZAD
Other Parts Discussed in Thread: CC3220S
HI,
What is the command use to jump from application to flash bootloader? is this the following function from boot_demo1 code?
//*****************************************************************************
//
// Passes control to the bootloader and initiates a remote software update.
//
// This function passes control to the bootloader and initiates an update of
// the main application firmware image via UART0 or USB depending
// upon the specific boot loader binary in use.
//
// \return Never returns.
//
//*****************************************************************************
void
JumpToBootLoader(void)
{
//
// We must make sure we turn off SysTick and its interrupt before entering
// the boot loader!
//
MAP_SysTickIntDisable();
MAP_SysTickDisable();
//
// Disable all processor interrupts. Instead of disabling them
// one at a time, a direct write to NVIC is done to disable all
// peripheral interrupts.
//
HWREG(NVIC_DIS0) = 0xffffffff;
HWREG(NVIC_DIS1) = 0xffffffff;
HWREG(NVIC_DIS2) = 0xffffffff;
HWREG(NVIC_DIS3) = 0xffffffff;
//
// Return control to the boot loader. This is a call to the SVC
// handler in the boot loader.
//
(*((void (*)(void))(*(uint32_t *)0x2c)))();
}
Thanks