Part Number: DK-TM4C129X
Other Parts Discussed in Thread: TM4C1292NCPDT
Dear all:
I want to used the uart rx interrupt mode.
And the sys/bios version is" bios_6_45_02_31".
When i add interrupt register funtion(UARTIntRegister(UART0_BASE,UARTIntHandler)),"program will not fit into available memory" will be occured after build the project.
How to resolve the error ? Do you have any suggestion?
Look forward to your reply.
*********************ERROR INFORMATION*************************************
Description Resource Path Location Type
<a href="file:/c:/ti/ccsv8/tools/compiler/dmed/HTML/10099.html">#10099-D</a> program will not fit into available memory. run placement with alignment fails for section ".vtable" size 0x26c , overlaps with ".vecs", size 0x360 (page 0) tm4c1292ncpdt.cmd /TivaTM4C129XNCPDT line 38 C/C++ Problem
***********************************************************************************
*********************CMD FILE**************************************************
--retain=g_pfnVectors
MEMORY
{
FLASH (RX) : origin = 0x00000000, length = 0x00100000
SRAM (RWX) : origin = 0x20000000, length = 0x00040000
}
/* The following command line options are set as part of the CCS project. */
/* If you are building using the command line, or for some reason want to */
/* define them here, you can uncomment and modify these lines as needed. */
/* If you are using CCS for building, it is probably better to make any such */
/* modifications in your CCS project and leave this file alone. */
/* */
/* --heap_size=0 */
/* --stack_size=256 */
/* --library=rtsv7M4_T_le_eabi.lib */
/* Section allocation in memory */
SECTIONS
{
.intvecs: > 0x00000000
.text : > FLASH
.const : > FLASH
.cinit : > FLASH
.pinit : > FLASH
.init_array : > FLASH
.vtable : > 0x20000000
.data : > SRAM
.bss : > SRAM
.sysmem : > SRAM
.stack : > SRAM
.TI.ramfunc : {} LOAD = FLASH,
RUN = SRAM,
LOAD_START(RamfuncsLoadStart),
LOAD_SIZE(RamfuncsLoadSize),
LOAD_END(RamfuncsLoadEnd),
RUN_START(RamfuncsRunStart),
RUN_SIZE(RamfuncsRunSize),
RUN_END(RamfuncsRunEnd),
PAGE = 0
}
__STACK_TOP = __stack + 512;
**********************************************************************************