Part Number: TM4C123BH6ZRB
Other Parts Discussed in Thread: UNIFLASH
Part: TM4C123BH6ZRB
Am using latest version of uniflash on Fedora Linux.
I can erase the Tiva via commandline:
/usr/local/uniflash_6.4.0/dslite.sh -e -c /tftpboot/sm400/Tiva_TM4C123BH6ZRB.ccxml -a Erase # ***** WORKS *****
I am able to reprogram the Tiva using the cumbersome uniflash GUI, using the same '.bin' file as below.
But cannot reflash via commandline: /usr/local/uniflash_6.4.0/dslite.sh -e -c /tftpboot/sm400/Tiva_TM4C123BH6ZRB.ccxml -f -v /tftpboot/sm400/sm400_bmc-01.18-01.18.bin # ***** BROKEN ***** Executing the following command: > /usr/local/uniflash_6.4.0/deskdb/content/TICloudAgent/linux/ccs_base/DebugServer/bin/DSLite flash -e -c /tftpboot/sm400/Tiva_TM4C123BH6ZRB.ccxml -f -v /tftpboot/sm400/sm400_bmc-01.18-01.18.bin For more details and examples, please refer to the UniFlash Quick Start guide. DSLite version 10.4.0.2437 Configuring Debugger (may take a few minutes on first launch)... Initializing Register Database... Initializing: CS_DAP_0 Executing Startup Scripts: CS_DAP_0 Initializing: CORTEX_M4_0 Executing Startup Scripts: CORTEX_M4_0 CORTEX_M4_0: GEL Output: Memory Map Initialization Complete Connecting... Failed: Encountered a problem loading file: /tftpboot/sm400/sm400_bmc-01.18-01.18.bin Could not determine target type of file Note: THERE IS NO QUICK START GUIDE file in the released files...