This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357-EP: Regarding verification of ESM1.40

Part Number: TMS570LC4357-EP

Hi,

This is a question regarding notification "ESM1.40".(ESM1.40 : ESM Group1 Channel40)
We are now testing the ESM function of TMS570 MCU on the evaluation board.
Based on explanation in Sec 38.3.2.4 of SPNU563A, we tried to force ESM 1.40 by using the following test codes.
But the test result was not as expected. The MCU notified no error.

/* ESM 1.40: EFCBOUND = 0x0013C000 */
efcREG->BOUND = (1U << 20) | (0xFU << 14);

Should we modify the test codes? Please advise.

Thanks,

Sho