Part Number: TMS570LS1224
Hello, Ti engineers. I want to know how the chip is configured to enter sleep mode and wake-up mode by software. Is there a relevant function interface or instruction? Or is there a corresponding demo program? thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LS1224
Hello, Ti engineers. I want to know how the chip is configured to enter sleep mode and wake-up mode by software. Is there a relevant function interface or instruction? Or is there a corresponding demo program? thanks
Hi Shuai:
Please take a look at my example:
This example is developed for LS0714, you can import it to LS1224 platform.
Hello,Ti engineers.I use your example to config the TMS570LS1224,but when it enter the sleep mode. It showed the following prompt:
CortexR4: Trouble Halting Target CPU: (Error -2064 @ 0x0) Unable to read device status. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.4.0.00129)
CortexR4: Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.4.0.00129)
And I don't know how to wake up it !
Hi Ziwen,
When the device is in sleep mode, the JTAG emulator is not able to connect to the device.
The device i sleep mode can be waked up through a GIO interrupt, a CAN message, and a SCI message. The my example uses a GIO interrupt to wake up the slept device.