Part Number: EK-TM4C123GXL
Other Parts Discussed in Thread: SW-TM4C
My Windows 10 Pro PC (build 19043.1165) does not detect the TM4C123GXL launchpad board when I plug it in via USB. There is no change in the device manager when the board is connected. I have attempted to manually load in the current ICDI drivers via add legacy hardware, but get an error code 10 for "This device cannot start."
The USB cable works and the board can be detected without problems on a different computer. I have also verified that I have it connected properly to the debug port and the switch is in the correct position as well.
For reference, I have SW-TM4C-2.2.0.295 installed, the latest ICDI drivers available, and am trying to use it with CCS 10.4.0.00006.