This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can not measure PWM via NHET

Other Parts Discussed in Thread: HALCOGEN

Hi folks,

I want to measure PWM signals but it does not work.

I configured NHET2 to generate a PWM signal. This works fine so far. Then I configured NHET4 as capture via HALCoGen. Finally I wired NHET2 with NHET4 and started my program. But nothing happens. I also checked the HETRAM but the data fields were 0 all the time.

My configuration:

HCLK: 160MHz
VCLK2: 80MHz
HRP: 5  ->  HR clock: 13Mhz
LRP: 3  ->  Loop Time: 1200ns
NHET2 as output
NHET4 as input

So, where is my mistake?