Part Number: TM4C123AE6PM
Hello,
There are efforts to try to enable a PSU primary and secondary firmware download function through CAN protocol. The TM4C123AE6PMI7R is used as the CAN BUS microcontroller and SN65HVD257DR as the CAN bus transceivers. There are a few questions we have:
Can the microcontroller support more than 8 bytes of write data? Can it support up to 32 bytes?
Can the data package extend from 8 bytes to 32 bytes (data 16 byte + header + check sum)?
Thank you.