Part Number: TMS570LS0432
Other Parts Discussed in Thread: HALCOGEN,
Hi, I am using the TMS570LS0432. I have generated the code from HALCoGen, which is name example_canCommunication.c.
I have done the same steps on the HALCoGen; however, it could not work when I debugged the microcontroller. The hardware connection is described.
Moreover, CAN-BUS shield V2.0 has been used for transceiving the message.
Rx-rx, tx-tx, 5V and GRN is connected.
With the help of CAN-H and CAN-L, pcan is connected to the computer.
I did not use to db9 port.
Also, I could not see the message from the terminal, Hercules tutorial: can communication video does not help me either.
I don't know where I am doing wrong. I would please request you to help me.