This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need help choosing microcontroller for system

Must haves:

Minimum flash memory of 128Kb
Minimum Clock Speed of 1MHz
Support for sleep/low power mode
Support for connection with H-bridge (it is supposed to control four components that needs up to 40V, 0.5A  via PWM)
Support for SD-card (or eMMC)
Need for 3 I/O channels (communication protocol is flexible, though RS232 is preferable)

Optimization variable:
Keeping power consumption low


If more information is necessary do reply