This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357-EP: Regarding Interconnect Self-test

Part Number: TMS570LC4357-EP

Hi,

This is a question regarding ESM3.12 and Interconnect Self-test.
We are now testing the ESM function of TMS570 MCU on the evaluation board.


We can success Interconnect Self-test using our created test code based on Sec 4.3.4 of SPNU563A.
For checked to notification of ESM3.12, Interconnect Self-test need to be fail.

Could you please tell me about how to fail Interconnect Self-test?

Thanks,

Sho

  • Hi,

     Did you follow the below sequence?

    Can you show your code sequence?

    Did you observe the CPU reset?

    Did you see any flags set in SDC_STATUS register? See below. Please also be aware of errata DEVICE#51 that the status will be left-shifted by 24 bits. 

    Can you show the ESM log?

  • Hi Charles-san,

    Thank you for your reply.

    Interconnect self-test is successful, and we would like to verify notification of ESM3.12,.

    My code sequence is below(using Hercules SafeTI Diagnostic Library V.2.4.0);

    1) SL_SelfTest_MemoryInterconnect(MEMINTRCNT_SELFTEST)

    2) CPU Reset

    3) SL_SelfTest_Status_MemIntrcntSelftest()

    Each status register of ESM and SDC is no error.

    ・ESM
    ESMSR1: 0x00000000
    ESMSR2: 0x00000000
    ESMSR3: 0x00000000
    ESMSR4: 0x00000000
    ESMSR7: 0x00000000
    ・SDC
    SDC_STATUS: 0x0A000000 - NT_OK(3) & PT_OK(1)

    Could you please tell me about technique of generating ESM3.12?
    Please advice.

    Thanks,

    Sho

  • Kobori-san,

      I think ESM3.12 is only asserted if the selftest fails. Since the selftest does not fail, no error signal is asserted to ESM module. You should read the PT_OK and NT_OK bits. If they are set, it means the selftest is done without errors. 

    4.3.4 Interconnect Self-test
    CPU Interconnect Subsystem can be put into self-test. When in self-test, the self-test logic will apply test
    stimulus to each master and slave interface. If an error is detected, the type of error for the corresponding
    interface is logged. An error is asserted to ESM Group 3 if the self-test does not complete successfully.
    NOTE: Application must only launch CPU Interconnect Subsystem self-test when there are no bus
    transactions from any masters including the CPU cores. While in self-test, the interconnect
    can not service any requests. Bus master requests can be lost or corrupted. It is recommend
    that the self-test is only exercised as part of the device initialization before any master is
    setup by the CPU.
    To launch the self-test, the applicable must follow the below sequence:
    1. Write 0xA key to the DTC_ERROR_RESET bits of the SCMCNTRL register in the SCM module.
    2. CPU executes WFI instruction to put itself in idle state. The start of self-test is gated by the idle state of
    the CPU.
    3. When both step 1 and 2 are met, the self-test will start. While self-test is on-going, the CPU cores is
    forced into reset. Note that reset is only held to the CPU cores while the rest of the system is not.
    4. When self-test is complete, the DTC_ERROR_RESET bits is automatically reverted back to 0x5 as the
    reset value.
    5. After the self-test is complete, a reset is applied to the CPU Interconnect Subsystem for 16 HCLK
    cycles. During this time, the CPU is also held in reset.
    6. After the interconnect and the CPU comes out of the reset, normal code execution can then start. CPU
    can check the self-test status by reading the NT_OK bit and the PT_OK bit of the SDC_STATUS
    register. These two bits indicate if the negative test and positive self-test sequence have passed. In
    addition, if the self-test has failed, the error is asserted to the ESM module.

  • Hi Charles-san,

    Thank you for your information.

    I understood ESM 3.12 should be occurred when Interconnect self-test failed.
    However, my test code invariably success interconnect self-test.

    I would like to verify notification of ESM 3.12, could you please tell me about forcibly technique of failing Interconnect self-test?

    Thanks,

    Sho

  • Hi Kobori-san,

      II'm sorry that I don't think there is a way to force the interconnect selftest to fail. I understand your desire to cause an intentional selftest failure so you can confirm and observe that the selftest is actually working. However, this is not the case. You can launch the selftest. If it truly fails then ESM3.12 will set.  

  • Hi Charles-san,

    Thank you for your support.

    Best regards,

    Sho