Part Number: MCU-PLUS-SDK-AM243X
Running CCS 10.4 under Windows 10 Pro, used Resource Explorer to install mcu_plus_sdk_am243x_08_00_00_21. Imported an example but got errors from the makefile_ccs_bootimage_gen:
Finished building target: "enet_lwip_cpsw_am243x-evm_r5fss0-0_freertos_ti-arm-clang.out" C:/ti/ccs1040/ccs/utils/bin/gmake -C C:\Users\mr_halfword\workspace_v10\enet_lwip_cpsw_am243x-evm_r5fss0-0_freertos_ti-arm-clang -f makefile_ccs_bootimage_gen OUTNAME=enet_lwip_cpsw_am243x-evm_r5fss0-0_freertos_ti-arm-clang PROFILE=Debug MCU_PLUS_SDK_PATH=C:/ti/mcu_plus_sdk_am243x_08_00_00_21 CG_TOOL_ROOT=C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-armllvm_1.3.0.LTS CCS_INSTALL_DIR=C:\ti\ccs1040\ccs CCS_IDE_MODE=desktop Boot image: am243x:r5fss0-0:freertos:ti-arm-clang C:/Users/mr_halfword/workspace_v10/enet_lwip_cpsw_am243x-evm_r5fss0-0_freertos_ti-arm-clang/Debug/enet_lwip_cpsw_am243x-evm_r5fss0-0_freertos_ti-arm-clang.appimage ... C:/ti/mcu_plus_sdk_am243x_08_00_00_21/tools/boot/out2rprc/out2rprc.exe Debug/enet_lwip_cpsw_am243x-evm_r5fss0-0_freertos_ti-arm-clang.out C:/Users/mr_halfword/workspace_v10/enet_lwip_cpsw_am243x-evm_r5fss0-0_freertos_ti-arm-clang/Debug/enet_lwip_cpsw_am243x-evm_r5fss0-0_freertos_ti-arm-clang.rprc_tmp >> Debug/temp_stdout_Debug.txt makefile_ccs_bootimage_gen:71: recipe for target 'all' failed gmake[3]: *** [all] Error -2146232576 gmake[2]: [post-build] Error 2 (ignored) makefile:181: recipe for target 'post-build' failed **** Build Finished ****
When attempted to run C:/ti/mcu_plus_sdk_am64x_08_00_00_21/tools/boot/out2rprc/out2rprc.exe from a command shell got:

Clicked "Download and install this feature" to let Windows 10 install the required .NET framework 3.5.
After the installation of .NET framework 3.5 was complete, the makefile_ccs_bootimage_gen then ran successfully.
The Download, Install and Setup SDK and Tools doesn't seem to mention that the .NET framework might need to be installed / updated under Windows 10 (it only mentions the need to install the Mono runtime if on Linux).
Is it worth updating the setup instructions to mention the required .NET framework version to be installed under Windows 10 for boot image generation?