Part Number: LP-AM243
Hello Guys,
Good day.
Our customer is using LP-AM243 together with a MAC OS. T
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LP-AM243
Hello Guys,
Good day.
Our customer is using LP-AM243 together with a MAC OS. The "out-of-the-box" experience cannot establish a connection with the board via the USB debug port. It says ports are available but never connects. He thought maybe it was missing a driver, so he install the IDE, but it also doesn't have support for the Sitara chip set. What could we be missing?
Thanks and regards,
Art
It says ports are available but never connects.
I had the same error, when trying to run the LP-AM243 together with Windows. Turns out the the LP-AM243 didn't have the SOC initialization binary pre-flashed. Following the information in LP-AM243: LP-AM243x was able to flash the SOC initialization binary and then the "out-of-the-box" experience connected.
Hello Guys,
Just like to update regarding this.
Best regards,
Art
Hi Art,
There is known limitation in AM243x/AM64x SOCs where you need to connect the JTAG cable only after board is powered ON.
Also please check if you have configured board in right boot mode and SOC init binaries flashed in the QSPI flash.
Regards,
Prasad
Hello Prasad,
I sent you a separate email regarding this.
Thanks and regards,
Art