Part Number: TMS570LC4357
On our new board, the designer gave me over-current detection on the dual-motor controller -- but they connected one TZ1_3 input for PWM1-3 and the second TZ1_3 input to the PWM4-6. The J3-TZ1_3 input properly trips PWMS1-6, but the D19-TZ1_3 input does not do anything. I have the PINMUX set for both pins to be TZ1_3, but I wonder if essentially ORing these pins together was invalid?
Note on the next board, we are separating the trip-zones (using TZ1_2 for PWMs4-6).
Thanks,
Jim