Part Number: RM44L920
Hello,
I have a question about the N2HET loopback function as it couples 2 HR structures to run a test over the digital or analog path.
If I do this, can I use the loopback function in simple GIO mode or is the N2HET structure expecting a PWM signal which is feed to the neigbour HR structure?
According to the TRM for the HETLBPSEL and HETLBPDIR registers, it states that "The pin which is not driven by the N2HET pin actions can still be used as normal GIO pin." - does that mean when I want to apply the test in GIO mode on the N2HET pins that the corresponding neighbour pin ( n+1) of the N2HET loopback pair which is used in a serial communiction context to provide for example a clocking signal stops to work? This pin can only be used in normal GIO mode instead, alternative functions derived from a different interface are not taken into account anymore when applying the test ?