Part Number: TMS570LC4357
The customer would like to know how to configure the dma to read the data in nvsram by connecting to the tms570lc4357 chip via emif.
Could you please help check this?
Thanks a lot!
Best Regards,
Cherry Zhou
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LC4357
The customer would like to know how to configure the dma to read the data in nvsram by connecting to the tms570lc4357 chip via emif.
Could you please help check this?
Thanks a lot!
Best Regards,
Cherry Zhou
Hi Cherry,
The DMA can be used to transfer words of data from memory attached to EMIF and MCU internal SRAM without any CPU load. The transfer of data is triggered by SW.
This is an example to copy data from one memory location to another memory location (EMIF Memory):
/** @file HL_sys_main.c
* @brief Application main file
* @date 11-Dec-2018
* @version 04.07.01
*
* This file contains an empty main function,
* which can be used for the application.
*/
/*
* Copyright (C) 2009-2018 Texas Instruments Incorporated - www.ti.com
*
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the
* distribution.
*
* Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
* "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
* LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
* A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
* OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
* SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
* LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
* DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
* THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
* (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
* OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*/
/* USER CODE BEGIN (0) */
/* USER CODE END */
/* Include Files */
#include "HL_sys_common.h"
/* USER CODE BEGIN (1) */
//#include "HL_emif.h"
#include "HL_sys_dma.h"
#include "HL_sys_core.h"
#include "HL_gio.h"
#include "HL_pinmux.h"
#include "HL_esm.h"
/* example data Pattern configuration */
#define E_COUNT 8 /*64, Element count*/
#define F_COUNT 32 /*16, Frame count*/
#define D_SIZE E_COUNT * F_COUNT
void loadDataPattern(uint32 psize, uint32* pptr, uint32 pattern);
#pragma SET_DATA_SECTION(".sharedRAM")
uint32 TXDATA_RAM0[D_SIZE]; /* transmit buffer in sys ram */
uint32 RXDATA_RAM0[D_SIZE]= {0}; /* receive buffer in sys ram */
uint32 TXDATA_RAM1[D_SIZE]; /* transmit buffer in sys ram */
uint32 RXDATA_RAM1[D_SIZE]= {0}; /* receive buffer in sys ram */
g_dmaCTRL g_dmaCTRLPKT1, g_dmaCTRLPKT2; /* dma control packet configuration stack */
#pragma SET_DATA_SECTION()
/* USER CODE END */
/** @fn void main(void)
* @brief Application main function
* @note This function is empty by default.
*
* This function is called after startup.
* The user can use this function to implement the application.
*/
/* USER CODE BEGIN (2) */
unsigned int Channel0_HBC_Flag;
unsigned int Channel1_HBC_Flag;
/* USER CODE END */
int main(void)
{
/* USER CODE BEGIN (3) */
/* enable IRQ interrupt */
/*clear ESM error*/
uint16 i, j=0;
gioInit();
_enable_IRQ();
Channel0_HBC_Flag = 0;
Channel0_HBC_Flag = 1;
//dmaREG->PTCRL = 0x03 | 0x1 << 3 | 0x1 << 18; /* prority scheme: rotation*/
/* - creating a data chunk in system ram to start with ... */
loadDataPattern(D_SIZE, &TXDATA_RAM0[0], 0x5A5A5A5A);
loadDataPattern(D_SIZE, &TXDATA_RAM1[0], 0x5B5B5B5B);
/* - configuring dma control packets */
g_dmaCTRLPKT1.SADD = (uint32)TXDATA_RAM0; /* source address */
//g_dmaCTRLPKT1.DADD = (uint32)(0x80000000); //(0x08078000); /* destination address; SDRAM */
g_dmaCTRLPKT1.DADD = (uint32)RXDATA_RAM0; //(0x08078000); /* destination address; SDRAM */
g_dmaCTRLPKT1.CHCTRL = 0; /* channel control */
g_dmaCTRLPKT1.FRCNT = F_COUNT; /* frame count */
g_dmaCTRLPKT1.ELCNT = E_COUNT; /* element count */
g_dmaCTRLPKT1.ELDOFFSET = 0; /* element destination offset */
g_dmaCTRLPKT1.ELSOFFSET = 0; /* element destination offset */
g_dmaCTRLPKT1.FRDOFFSET = 0; /* frame destination offset */
g_dmaCTRLPKT1.FRSOFFSET = 0; /* frame destination offset */
g_dmaCTRLPKT1.PORTASGN = PORTA_READ_PORTA_WRITE;
g_dmaCTRLPKT1.RDSIZE = ACCESS_32_BIT; /* read size */
g_dmaCTRLPKT1.WRSIZE = ACCESS_32_BIT; /* write size */
g_dmaCTRLPKT1.TTYPE = FRAME_TRANSFER ; /* transfer type */
g_dmaCTRLPKT1.ADDMODERD = ADDR_INC1; /* address mode read */
g_dmaCTRLPKT1.ADDMODEWR = ADDR_INC1; /* address mode write */
g_dmaCTRLPKT1.AUTOINIT = AUTOINIT_ON; /* autoinit */
//g_dmaCTRLPKT2.SADD = (uint32)(0x80001000); //0x08076000); /* source address */
g_dmaCTRLPKT2.SADD = (uint32)TXDATA_RAM1; //0x08076000); /* source address */
g_dmaCTRLPKT2.DADD = (uint32)RXDATA_RAM1; /* destination address */
g_dmaCTRLPKT2.CHCTRL = 0; /* channel control */
g_dmaCTRLPKT2.FRCNT = F_COUNT; /* frame count */
g_dmaCTRLPKT2.ELCNT = E_COUNT; /* element count */
g_dmaCTRLPKT2.ELDOFFSET = 0; /* element destination offset */
g_dmaCTRLPKT2.ELSOFFSET = 0; /* element destination offset */
g_dmaCTRLPKT2.FRDOFFSET = 0; /* frame destination offset */
g_dmaCTRLPKT2.FRSOFFSET = 0; /* frame destination offset */
g_dmaCTRLPKT2.PORTASGN = PORTA_READ_PORTA_WRITE;
g_dmaCTRLPKT2.RDSIZE = ACCESS_32_BIT; /* read size */
g_dmaCTRLPKT2.WRSIZE = ACCESS_32_BIT; /* write size */
g_dmaCTRLPKT2.TTYPE = FRAME_TRANSFER ; /* transfer type */
g_dmaCTRLPKT2.ADDMODERD = ADDR_INC1; /* address mode read */
g_dmaCTRLPKT2.ADDMODEWR = ADDR_INC1; /* address mode write */
g_dmaCTRLPKT2.AUTOINIT = AUTOINIT_ON; /* autoinit */
/* - setting dma control packets */
dmaSetCtrlPacket(DMA_CH1, g_dmaCTRLPKT1); //tx
dmaSetCtrlPacket(DMA_CH0, g_dmaCTRLPKT2); //rx
/* - setting the dma channel to trigger on h/w request */
dmaSetChEnable(DMA_CH1, DMA_SW);
dmaSetChEnable(DMA_CH0, DMA_SW);
/* Enable Block Transfer Complete interrupt for the receive after transfer complete */
dmaEnableInterrupt(DMA_CH0, FTC, DMA_INTA);
dmaEnableInterrupt(DMA_CH1, FTC, DMA_INTA);
dmaEnable();
for(i=1; i<F_COUNT; i++)
{
dmaSetChEnable(DMA_CH1, DMA_SW);
dmaSetChEnable(DMA_CH0, DMA_SW);
j = i;
}
while(1); /* loop forever */
/* USER CODE END */
return 0;
}
/* USER CODE BEGIN (4) */
/** void loadDataPattern(uint32 psize, uint16* pptr)
*/
void loadDataPattern(uint32 psize, uint32* pptr, uint32 pattern)
{
int i;
for(i=0;i<psize;i++)
{
*(pptr++) = pattern + i;
}
}
/**************************************************************************//**
* DMA Interrupt
*****************************************************************************/
void dmaGroupANotification(dmaInterrupt_t inttype, uint32 channel)
{
/* enter user code between the USER CODE BEGIN and USER CODE END. */
if(channel ==0){
Channel0_HBC_Flag = 1;
}
if(channel == 1){
Channel1_HBC_Flag = 1;
}
}
/* USER CODE END */