Part Number: RM48L952
Other Parts Discussed in Thread: HALCOGEN
Hi Ti,
Below are our doubts about the usage of the safety diag library.
1. For some safety features/diagnostic, SafeTI library provides the API name. But for some cases, CLK1(Low Power Oscillator Clock Detector ), CLK2 (External monitoring via ECLK ) and CLK5C (External watchdog) it Is mentioned as "handled by safety application". Does it mean, user application has to configure/enable those tests in SW, HW, and system?
2. In the above case, If the tests are SW dependent, is there any example code available?
3. For some diagnostics, CLK6 (Periodic software readback of static clock configuration registers) and CLK7 (Software readback of written configuration). What is the difference between both and how to implement it in the user application?
4. What does it mean "7.133 Use of DCC as Program Sequence Watchdog"? Does it is diagnostic for N2HET/DCC module or is this a diagnostics equivalent/same as an Internal or external watchdog (CLK5x) diagnostics?
Regards,
Monish