Part Number: MSP432E401Y
Other Parts Discussed in Thread: MSP432E411Y
Hai,
it is possible to use msp432e411y as spi master and arduino as spi slave,
to test for qssi module working.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP432E401Y
Other Parts Discussed in Thread: MSP432E411Y
Hai,
it is possible to use msp432e411y as spi master and arduino as spi slave,
to test for qssi module working.
Hi,
You can configure the QSSI module to work in Freescale SPI Frame Format. The MSP432E4 Technical Reference Manual can provide further details on the Freescale SPI Frame Format (Section 23.3.7.2).
Regards,
Luke
Hi,
I have one doubt , regrading SSInFSS pin ,
whether ,this pin will go automatically low ,during byte transfer,
or we need to manually make this pin low,
I feel confused while reading datasheet.
pls reply
Thanks
Regards.
Rajeshkumar
Hi Rajeshjumar,
For the freescale format the SSInFSS signal behaves as your peripheral select (peripheral is the slave device). Section 23.3.7.2

And depending on the configuration you choose different settings will be made. I highly suggest looking at this section to understand the different configurations that are available. The term forced is used as it will automatically set, looking at the timing diagrams should help depict it. You can verify this though by looking at the registers through CCS.
Regards,
Luke
Hi, Luke
How to check , qssi is transferring data or not , any methods available apart from
checking register using ccs.
Regards
Rajeshkumar
Hi Rajeshkumar,
You should be able to connect an scope to the SSI pins to see the signals on the lines. Below is an image taken from the Datasheet that lists the SSI pins.

Regards,
Luke