Part Number: TM4C1294NCPDT
Hi,
I am having a strange issue where I use daisy chained TM4C1294NCDPT devices. The problem occurs when accessing the JTAG chain through XDS110 and CCS 10.2. It seems as if the boundary scan on the second device is active even though I am just using the TAP to download code or debug. As I understand it the XDS110 startup sequence should disable the boundary scan functionality at first connection. Still I have input pins suddenly turning to outputs or pull-up on my second device. Debugging and loading code is fine. When using the XDS 200 debugger everything works.
The issue is not urgent since I can use the XDS 200 instead. Just curious if there is a bug in the XDS 110 or in my setup.
Best regards
Jens