Part Number: TMS570LC4357-EP
Hello everyone,
for our project we use the TMS570LC4357-EP programming it in bare metal with only single task, so we don't use an O.S. or multitask programming. Our customer asks us which is the approch in order to use the dual core lockstep. Our first answer is that we aren't intended to use the lockstep ignornig the ESM signalation. After that they asked a second question, they undrestood we are using the uC with only one core and they would like a demonstration which process will be carried out to ensure that the second core will be not operative.
Reading the user manual, we didn't find any reference about the single or dual core programming.
I have some questions:
1) Is it possible to use only one core forcing the programmation?
2) if yes, how can i configure the uC?
3) Where can i find these information?
4) how can I obtain information on CCS if my embedded application runs in single or dual core?
Thank you for your support.
Best regards.
Domenico