Part Number: MSP432E401Y
Other Parts Discussed in Thread: BOOSTXL-SHARP128
Team,
I have tried using the FATSD RAW example for reading/writing to SDXC type cards formatted with EXFAT file system.
I have modified the ffconf.h
#define FF_USE_LFN 3 #define FF_FS_EXFAT 1
After recompiling the FATFS library

When LFN is enable, during the FATFS library calls in the main application (fatsdraw example) gets a faultISR, or if it is ran in RTOS environment, it throws HWI exception.
Is there a successful example of EXFAT support on any SimpleLink device? It could be CC3220, CC3225, CC1352, etc.
If there is a working example I can debug and find the issue.
Nima