Hi,
My main problem is while debugging; the software debug process has suddenly stopped. It must be debugging all the time. However, sometimes it stops in 1 second or more than 1 second, rarely does not stop. I want to debug the software until I stopped the program. Moreover, when it stopped, I have to be seen values between 0-1 from the expression table because those values are flagged; however after debugging process is stopped, those values can be seen as another value. Therefore, I need to terminate to program and again click debug. Moreover, when it stopped if I clicked the resume button I took that warning and expression table below.
Thank you,
Özden