Part Number: MSP-EXP432E401Y
Other Parts Discussed in Thread: DAC61402, DAC81404, DAC81404EVM
Hi,
I got the MSP-EXP432E401Y to use with BP-DAC61402EVM and, I tried to use https://dev.ti.com/uniflash but it doesn't work, I tried also to download it from the GUI composer Galley but it also doesn't work.
1) is it a must to do a firmware upgrade? it's not very clear which jumper I need to remove. The figure is different as MSP-EXP432E401Y (2.2.1 BP-DAC81404EVM USER Guide)
1)Do you have any software to use this device, link to download? I want to use it to change the output voltage from BP-DAC61402EVM by the computer
2) There are 2 USB ports, is one of them for power supply and the other for communication? when I connect the MSP-EXP432E401Y to the computer the device manager recognizes it as XDS110 (02.03.00.09) Embed with CMISIS-DAP and the driver not installed. where I can download the drivers that I need?
Regards,
Avi