This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

does RTI include in the TMS570 R4F core?



my question is :

1. Does RTI module is in the TMS570 R4F core?  or just a peripheral linked to the cpu internal bus like DCAN or SCI/LIN module?

2. If RTI is a part of R4F core, are there two entity of RTI with two entity R4F core? In my safety application the time tick is safety critical.

3. If RTI isn't a part of R4F core, Die failure Rate for RTI Subsystems isn't list in Certificate document.

thx.

  •  

    Yang,

    Find below my answers:

    1. No. It's not part of core, but a system module.

    2. No.

    3. I need to check. But there are two counters within RTI. (FRC0 and FRC1) which can be made use of.

        I haven't heard of any issues with RTI so far when the RTI clock settings are done as per TI recommendations.

    Best Regards,

    Pratip

     

     

  • On 3.

    We make the assumption that pretty much every application would make use of the RTI. Thus the RTI block is considered a part of "Subsystem Common for all SIFs" and so the failure rate is included in the failure rate of that subsystem.

    - Abhishek