Part Number: MCU-PLUS-SDK-AM243X
Hello e2e,
We have a question about the SYSFW address in CPU internal SRAM, the SYSFW is included from the file "C:\ti\mcu_plus_sdk_am243x_08_00_00_21\source\drivers\sciclient\soc\am64x_am243x\sysfw_signed.h", and loaded by Sciclient_loadFirmware((uint32_t*)gSysFw), but we can not find the real address in CPU RAM, can you help on that?
Thanks in advance.
void Bootloader_socLoadSysFw()
{
uint32_t size = SYSFW_SIZE_IN_BYTES;
int32_t retVal = SystemP_SUCCESS;
retVal = Sciclient_init(CSL_CORE_ID_R5FSS0_0);
if(retVal == SystemP_SUCCESS)
{
size = (size + 31U) & ~(31U);
CacheP_wbInv( (void*)gSysFw, size, CacheP_TYPE_ALL);
retVal = Sciclient_loadFirmware((uint32_t*)gSysFw);
}
if(retVal == SystemP_SUCCESS)
{
retVal = sciclient_set_boardcfg();
}
DebugP_assertNoLog(retVal==SystemP_SUCCESS);
}
LEON