Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: SYSBIOS
Hi,
We are using TM4C1294NCPDT TCP using RTOS, Please find the attached source code for your kind reference.
When the LAN cable is connected system is functioning as per requirements.
When ever the LAN cable disconnected and reconnected system is not getting connected to server until we power restart the device.
We are using two different tasks to connect different ports as (5000 and 5001).
Other than this issue system is working fine.
Can you guide us how to fix this issue on priority basis.
Void tcpHandler(UArg arg0, UArg arg1)
{
SOCKET lSocket;
int status;
struct sockaddr_in sLocalAddr;
int clientfd;
int temp,temp1;
int txbytes;
int txlen;
int optval;
int optlen = sizeof(optval);
int reuse = 1;
WD_Flag ^= true;
fdOpenSession(TaskSelf());
lSocket = socket(AF_INET, SOCK_STREAM, IPPROTO_TCP);
if (lSocket < 0) {
System_printf("tcpHandler: socket failed\n");
Task_exit();
return;
}
memset((char *)&sLocalAddr, 0, sizeof(sLocalAddr));
sLocalAddr.sin_family = AF_INET;//
sLocalAddr.sin_addr.s_addr = inet_addr(Server_IP_Address);//inet_addr("10.7.55.2");////inet_addr("192.168.0.125");//htonl(INADDR_ANY);
sLocalAddr.sin_port = htons(arg0);
sprintf (TCP_Send_Buffer, "%c", '$');
sprintf (TCP_Send_Buffer+1, "%c", ',');
usprintf(TCP_Send_Buffer+2, "%d.%d.%d.%d", Ip_Address_Static & 0xff, (Ip_Address_Static >> 8) & 0xff,
(Ip_Address_Static >> 16) & 0xff, (Ip_Address_Static >> 24) & 0xff);
sprintf (TCP_Send_Buffer+strlen(TCP_Send_Buffer), "%c", ',');
temp = (char)(sLocalAddr.sin_port >> 8) & 0xff;
temp1 = (char)(sLocalAddr.sin_port & 0xff);
temp = (int)(temp1 << 8) | temp;
usprintf(TCP_Send_Buffer+strlen(TCP_Send_Buffer), "%d", temp);//,
sprintf (TCP_Send_Buffer+strlen(TCP_Send_Buffer), "%c", ',');
Frame_len = strlen(TCP_Send_Buffer);
while(clientfd = (connect(lSocket, (struct sockaddr *)&sLocalAddr, sizeof(sLocalAddr)) < 0)){
SysCtlDelay(g_ui32SysClock/100/3);
System_printf("Connection failed.\n%d", errno);
}
System_flush();
if (setsockopt(lSocket, SOL_SOCKET, SO_REUSEPORT, (const char*)&reuse, sizeof(reuse)) < 0)
perror("setsockopt(SO_REUSEPORT) failed");
status = bind(lSocket, (struct sockaddr *)&sLocalAddr, sizeof(sLocalAddr));
if (status == -1) {
System_printf("Error: bind failed.\n");
}
optval = 2;
if (setsockopt(lSocket, SOL_SOCKET, SO_RCVTIMEO, &optval, optlen) < 0) {
System_printf("Error: setsockopt failed\n");
}
while (true) {
MAP_GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_5,
(MAP_GPIOPinRead(GPIO_PORTN_BASE, GPIO_PIN_5) ^
GPIO_PIN_5));
if (Semaphore_getCount(semHandle) == 0) {
System_printf("Sem blocked in TCP Sender \n");
}
Semaphore_pend(semHandle, BIOS_NO_WAIT);
WD_Flag ^= true;
if((recv_comp == 0)&&(send_rns_details == 0)&&(send_bss_details == 0)&&(send_rs_details == 0)&&
(send_bs_details == 0)&&(send_fs_details == 0)&&(send_sp_details == 0)&&(send_config_details == 0)&&
(send_device_ip == 0)&&(send_server_ip == 0)){
if(Power_Reset == 0){
memset(TCP_Config_transmit_buf,0x00,150);
usprintf (TCP_Config_transmit_buf, "%c%c%s%c%s%c%c%c%c",
'$',',',Device_IP_Address, ',',"Connection_Check_with_Server",',','\r',',','\n');
txbytes = send(lSocket, (char *)TCP_Config_transmit_buf,strlen(TCP_Config_transmit_buf),0);
if(txbytes == strlen(TCP_Config_transmit_buf)){
send_server_ip = 0;
}
else;
close(clientfd);
Task_sleep(1000);
}
else;
}
resource = 0;
Semaphore_post(semHandle);
Task_sleep(1);
}
}
Void tcpHandler2(UArg arg0, UArg arg1)
{
SOCKET socketl;
int status;
struct sockaddr_in sLocalAddr;
int clientfd;
int nbytes;
int optval;
int optlen = sizeof(optval);
char ip_len=0;
char trecvbuffer[20];
int c = 0;
int c1 = 0;
char B_Rate[10];
char dlen,Receive_Fram_Len;
char *eptr;
uint32_t e2size,e2block,returnCode;
int reuse = 1;
int counter = 0;
WD_Flag ^= true;
fdOpenSession(TaskSelf());
socketl = socket(AF_INET, SOCK_STREAM, IPPROTO_TCP);
if (socketl < 0) {
System_printf("tcpHandler: socket failed\n");
Task_exit();
return;
}
memset((char *)&sLocalAddr, 0, sizeof(sLocalAddr));
sLocalAddr.sin_family = AF_INET;
sLocalAddr.sin_addr.s_addr = inet_addr(Server_IP_Address);//inet_addr("10.7.55.2");//inet_addr("10.7.55.85");////inet_addr("192.168.0.125");//inet_addr(Server_IP_Recv_Buf);////inet_addr("192.168.0.125");//htonl(INADDR_ANY);
sLocalAddr.sin_port = htons(arg0);
while(clientfd = (connect(socketl, (struct sockaddr *)&sLocalAddr, sizeof(sLocalAddr)) < 0)){
SysCtlDelay(g_ui32SysClock/100/3);
}
System_flush();
if (setsockopt(socketl, SOL_SOCKET, SO_REUSEPORT, (const char*)&reuse, sizeof(reuse)) < 0)
perror("setsockopt(SO_REUSEPORT) failed");
status = bind(socketl, (struct sockaddr *)&sLocalAddr, sizeof(sLocalAddr));
if (status == -1) {
System_printf("Error: bind failed.\n");
}
optval = 2;
if (setsockopt(socketl, SOL_SOCKET, SO_RCVTIMEO, &optval, optlen) < 0) {
System_printf("Error: setsockopt failed\n");
}
optval = 1;
if (setsockopt(socketl, SOL_SOCKET, SO_SNDTIMEO, &optval, optlen) < 0) {
System_printf("Error: setsockopt failed\n");
}
while (true) {
MAP_GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_5,
(MAP_GPIOPinRead(GPIO_PORTN_BASE, GPIO_PIN_5) ^
GPIO_PIN_5));
WD_Flag ^= true;
send(socketl, (char *)"$OK",3,0);
if (Semaphore_getCount(semHandle) == 0) {
System_printf("Sem blocked in TCP Receiver \n");
}
Semaphore_pend(semHandle, BIOS_NO_WAIT);
nbytes = recv(socketl, (char *)recvbuffer, TCPPACKETSIZE, 0);
if(nbytes > 1){
ip_len = strlen(Device_IP_Address);
}
if (connect(socketl, (struct sockaddr *)&sLocalAddr, sizeof(sLocalAddr)) < 0){
System_printf("DID NOT CONNECT \n");
System_printf("%d\n", fdError());
System_printf("Connection failed.\n%d", errno);
}
else {
System_printf("CONNECTED \n");
}
resource = 0;
Semaphore_post(semHandle);
Task_sleep(3);
}
}
Void functionNetworkOpenHook(Void)
{
char *HostName = "_csl_";
CI_IPNET NA;
CI_ROUTE RT;
HANDLE hCfg;
HANDLE hCfgIpAddr;
/* Setup manual IP address */
bzero(&NA, sizeof(NA));
NA.IPAddr = Ip_Address_Static;//inet_addr("192.168.0.143");//
strcpy(NA.Domain, "demo.net");
NA.NetType = 0;
Ip_Address = NA.IPAddr;
/* get the current static IP entry */
CfgGetEntry(0, CFGTAG_IPNET, 1, 1, &hCfgIpAddr);
/* remove the current static IP entry */
CfgRemoveEntry(0, hCfgIpAddr);
/* add a new static IP entry */
CfgAddEntry(0, CFGTAG_IPNET, 1, 0,
sizeof(CI_IPNET), (UINT8 *)&NA, 0);
bzero( &RT, sizeof(RT) );
RT.IPDestAddr = 0;//Ip_Address_Static;
RT.IPDestMask = subnetmaskaddress;
RT.IPGateAddr = GateWayAddress;//inet_addr("10.7.55.254");
hCfg = CfgNew();
CfgAddEntry( hCfg, CFGTAG_SYSINFO, CFGITEM_DHCP_HOSTNAME, 0,
strlen(HostName), (UINT8 *)HostName, 0 );
// Add the route
CfgAddEntry( hCfg, CFGTAG_ROUTE, 0, 0, sizeof(CI_ROUTE), (UINT8 *)&RT, 0 );
Error_Block eb;
/* Make sure Error_Block is initialized */
Error_init(&eb);
}
void main (void)
{
bool bUpdate;
uint32_t e2size,e2block,returnCode;
Error_Block eb;
Task_Handle taskHandle;
Task_Params taskParams;
Watchdog_Params params;
Semaphore_Params semParams;
WD_Flag ^= true;
Board_initGeneral();
Board_initGPIO();
Board_initEMAC();
Board_initI2C();
Board_initUART();
Board_initWatchdog();
g_ui32SysClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
SYSCTL_OSC_MAIN | SYSCTL_USE_PLL |
SYSCTL_CFG_VCO_480), 120000000);
Task_Params_init(&taskParams);
Error_init(&eb);
Semaphore_Params sem_params;
Semaphore_Params_init(&sem_params);
sem_params.mode = Semaphore_Mode_BINARY;
Semaphore_Handle sem = Semaphore_create(0, &sem_params, &eb);
if (sem == NULL) {
System_printf("Semaphore_create() failed!");
}
taskParams.stackSize = 2048;
taskParams.instance->name = "TCP";
taskParams.priority = 3;
taskParams.arg0 = TCPPORT;
taskHandle = Task_create((Task_FuncPtr)tcpHandler, &taskParams, &eb);
if (taskHandle == NULL) {
System_printf("Error: Failed to create new TCP Task\n");
System_flush();
}
taskParams.stackSize = 1536;
taskParams.instance->name = "TCP";
taskParams.priority = 1;
taskParams.arg0 = TCPPORT1;
taskHandle = Task_create((Task_FuncPtr)tcpHandler2, &taskParams, &eb);
if (taskHandle == NULL) {
System_printf("Error: Failed to create new TCP Task\n");
System_flush();
}
/* Construct a Semaphore object to be use as a resource lock, inital count 1 */
Semaphore_Params_init(&semParams);
Semaphore_construct(&semStruct, 1, &semParams);
/* Obtain instance handle */
semHandle = Semaphore_handle(&semStruct);
/* We want to sleep for 10000 microseconds */
sleepTickCount = 10000 / Clock_tickPeriod;
BIOS_start();
return (0);
}
/*
* Copyright (c) 2015-2016, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*/
/* ================ Clock configuration ================ */
var Clock = xdc.useModule('ti.sysbios.knl.Clock');
var GIO = xdc.useModule('ti.sysbios.io.GIO');
/*
* Default value is family dependent. For example, Linux systems often only
* support a minimum period of 10000 us and multiples of 10000 us.
* TI platforms have a default of 1000 us.
*/
Clock.tickPeriod = 1000;
/* ================ Defaults (module) configuration ================ */
var Defaults = xdc.useModule('xdc.runtime.Defaults');
/*
* A flag to allow module names to be loaded on the target. Module name
* strings are placed in the .const section for debugging purposes.
*
* Pick one:
* - true (default)
* Setting this parameter to true will include name strings in the .const
* section so that Errors and Asserts are easier to debug.
* - false
* Setting this parameter to false will reduce footprint in the .const
* section. As a result, Error and Assert messages will contain an
* "unknown module" prefix instead of the actual module name.
*/
Defaults.common$.namedModule = true;
//Defaults.common$.namedModule = false;
/* ================ Error configuration ================ */
var Error = xdc.useModule('xdc.runtime.Error');
/*
* This function is called to handle all raised errors, but unlike
* Error.raiseHook, this function is responsible for completely handling the
* error with an appropriately initialized Error_Block.
*
* Pick one:
* - Error.policyDefault (default)
* Calls Error.raiseHook with an initialized Error_Block structure and logs
* the error using the module's logger.
* - Error.policySpin
* Simple alternative that traps on a while(1) loop for minimized target
* footprint.
* Using Error.policySpin, the Error.raiseHook will NOT called.
*/
Error.policyFxn = Error.policyDefault;
//Error.policyFxn = Error.policySpin;
/*
* If Error.policyFxn is set to Error.policyDefault, this function is called
* whenever an error is raised by the Error module.
*
* Pick one:
* - Error.print (default)
* Errors are formatted and output via System_printf() for easier
* debugging.
* - null
* Errors are not formatted or logged. This option reduces code footprint.
* - non-null function
* Errors invoke custom user function. See the Error module documentation
* for more details.
*/
Error.raiseHook = Error.print;
//Error.raiseHook = null;
//Error.raiseHook = "&myErrorFxn";
/*
* If Error.policyFxn is set to Error.policyDefault, this option applies to the
* maximum number of times the Error.raiseHook function can be recursively
* invoked. This option limits the possibility of an infinite recursion that
* could lead to a stack overflow.
* The default value is 16.
*/
Error.maxDepth = 2;
/* ================ Hwi configuration ================ */
var halHwi = xdc.useModule('ti.sysbios.hal.Hwi');
var m3Hwi = xdc.useModule('ti.sysbios.family.arm.m3.Hwi');
/*
* Checks for Hwi (system) stack overruns while in the Idle loop.
*
* Pick one:
* - true (default)
* Checks the top word for system stack overflows during the idle loop and
* raises an Error if one is detected.
* - false
* Disabling the runtime check improves runtime performance and yields a
* reduced flash footprint.
*/
halHwi.checkStackFlag = true;
//halHwi.checkStackFlag = false;
/*
* The following options alter the system's behavior when a hardware exception
* is detected.
*
* Pick one:
* - Hwi.enableException = true
* This option causes the default m3Hwi.excHandlerFunc function to fully
* decode an exception and dump the registers to the system console.
* This option raises errors in the Error module and displays the
* exception in ROV.
* - Hwi.enableException = false
* This option reduces code footprint by not decoding or printing the
* exception to the system console.
* It however still raises errors in the Error module and displays the
* exception in ROV.
* - Hwi.excHandlerFunc = null
* This is the most aggressive option for code footprint savings; but it
* can difficult to debug exceptions. It reduces flash footprint by
* plugging in a default while(1) trap when exception occur. This option
* does not raise an error with the Error module.
*/
m3Hwi.enableException = true;
//m3Hwi.enableException = false;
//m3Hwi.excHandlerFunc = null;
/*
* Enable hardware exception generation when dividing by zero.
*
* Pick one:
* - 0 (default)
* Disables hardware exceptions when dividing by zero
* - 1
* Enables hardware exceptions when dividing by zero
*/
m3Hwi.nvicCCR.DIV_0_TRP = 0;
//m3Hwi.nvicCCR.DIV_0_TRP = 1;
/*
* Enable hardware exception generation for invalid data alignment.
*
* Pick one:
* - 0 (default)
* Disables hardware exceptions for data alignment
* - 1
* Enables hardware exceptions for data alignment
*/
m3Hwi.nvicCCR.UNALIGN_TRP = 0;
//m3Hwi.nvicCCR.UNALIGN_TRP = 1;
/* ================ Idle configuration ================ */
var Idle = xdc.useModule('ti.sysbios.knl.Idle');
/*
* The Idle module is used to specify a list of functions to be called when no
* other tasks are running in the system.
*
* Functions added here will be run continuously within the idle task.
*
* Function signature:
* Void func(Void);
*/
//Idle.addFunc("&myIdleFunc");
/* ================ Kernel (SYS/BIOS) configuration ================ */
var BIOS = xdc.useModule('ti.sysbios.BIOS');
/*
* Enable asserts in the BIOS library.
*
* Pick one:
* - true (default)
* Enables asserts for debugging purposes.
* - false
* Disables asserts for a reduced code footprint and better performance.
*/
//BIOS.assertsEnabled = true;
BIOS.assertsEnabled = false;
/*
* Specify default heap size for BIOS.
*/
BIOS.heapSize = 20480;
/*
* A flag to determine if xdc.runtime sources are to be included in a custom
* built BIOS library.
*
* Pick one:
* - false (default)
* The pre-built xdc.runtime library is provided by the respective target
* used to build the application.
* - true
* xdc.runtime library souces are to be included in the custom BIOS
* library. This option yields the most efficient library in both code
* footprint and runtime performance.
*/
BIOS.includeXdcRuntime = false;
//BIOS.includeXdcRuntime = true;
/*
* The SYS/BIOS runtime is provided in the form of a library that is linked
* with the application. Several forms of this library are provided with the
* SYS/BIOS product.
*
* Pick one:
* - BIOS.LibType_Custom
* Custom built library that is highly optimized for code footprint and
* runtime performance.
* - BIOS.LibType_Debug
* Custom built library that is non-optimized that can be used to
* single-step through APIs with a debugger.
*
*/
BIOS.libType = BIOS.LibType_Custom;
//BIOS.libType = BIOS.LibType_Debug;
/*
* Runtime instance creation enable flag.
*
* Pick one:
* - true (default)
* Allows Mod_create() and Mod_delete() to be called at runtime which
* requires a default heap for dynamic memory allocation.
* - false
* Reduces code footprint by disallowing Mod_create() and Mod_delete() to
* be called at runtime. Object instances are constructed via
* Mod_construct() and destructed via Mod_destruct().
*/
BIOS.runtimeCreatesEnabled = true;
//BIOS.runtimeCreatesEnabled = false;
/*
* Enable logs in the BIOS library.
*
* Pick one:
* - true (default)
* Enables logs for debugging purposes.
* - false
* Disables logging for reduced code footprint and improved runtime
* performance.
*/
//BIOS.logsEnabled = true;
BIOS.logsEnabled = false;
/* ================ Memory configuration ================ */
var Memory = xdc.useModule('xdc.runtime.Memory');
/*
* The Memory module itself simply provides a common interface for any
* variety of system and application specific memory management policies
* implemented by the IHeap modules(Ex. HeapMem, HeapBuf).
*/
/* ================ Program configuration ================ */
/*
* Program.stack is ignored with IAR. Use the project options in
* IAR Embedded Workbench to alter the system stack size.
*/
if (!Program.build.target.$name.match(/iar/)) {
/*
* Reducing the system stack size (used by ISRs and Swis) to reduce
* RAM usage.
*/
Program.stack = 1024;
}
/*
* Enable Semihosting for GNU targets to print to CCS console
*/
if (Program.build.target.$name.match(/gnu/)) {
var SemiHost = xdc.useModule('ti.sysbios.rts.gnu.SemiHostSupport');
}
/* ================ Semaphore configuration ================ */
var Semaphore = xdc.useModule('ti.sysbios.knl.Semaphore');
/*
* Enables global support for Task priority pend queuing.
*
* Pick one:
* - true (default)
* This allows pending tasks to be serviced based on their task priority.
* - false
* Pending tasks are services based on first in, first out basis.
*
* When using BIOS in ROM:
* This option must be set to false.
*/
//Semaphore.supportsPriority = true;
Semaphore.supportsPriority = false;
/*
* Allows for the implicit posting of events through the semaphore,
* disable for additional code saving.
*
* Pick one:
* - true
* This allows the Semaphore module to post semaphores and events
* simultaneously.
* - false (default)
* Events must be explicitly posted to unblock tasks.
*
*/
//Semaphore.supportsEvents = true;
Semaphore.supportsEvents = false;
/* ================ Swi configuration ================ */
var Swi = xdc.useModule('ti.sysbios.knl.Swi');
/*
* A software interrupt is an object that encapsulates a function to be
* executed and a priority. Software interrupts are prioritized, preempt tasks
* and are preempted by hardware interrupt service routines.
*
* This module is included to allow Swi's in a users' application.
*/
/* ================ System configuration ================ */
var System = xdc.useModule('xdc.runtime.System');
/*
* The Abort handler is called when the system exits abnormally.
*
* Pick one:
* - System.abortStd (default)
* Call the ANSI C Standard 'abort()' to terminate the application.
* - System.abortSpin
* A lightweight abort function that loops indefinitely in a while(1) trap
* function.
* - A custom abort handler
* A user-defined function. See the System module documentation for
* details.
*/
System.abortFxn = System.abortStd;
//System.abortFxn = System.abortSpin;
//System.abortFxn = "&myAbortSystem";
/*
* The Exit handler is called when the system exits normally.
*
* Pick one:
* - System.exitStd (default)
* Call the ANSI C Standard 'exit()' to terminate the application.
* - System.exitSpin
* A lightweight exit function that loops indefinitely in a while(1) trap
* function.
* - A custom exit function
* A user-defined function. See the System module documentation for
* details.
*/
System.exitFxn = System.exitStd;
//System.exitFxn = System.exitSpin;
//System.exitFxn = "&myExitSystem";
/*
* Minimize exit handler array in the System module. The System module includes
* an array of functions that are registered with System_atexit() which is
* called by System_exit(). The default value is 8.
*/
System.maxAtexitHandlers = 2;
/*
* The System.SupportProxy defines a low-level implementation of System
* functions such as System_printf(), System_flush(), etc.
*
* Pick one pair:
* - SysMin
* This module maintains an internal configurable circular buffer that
* stores the output until System_flush() is called.
* The size of the circular buffer is set via SysMin.bufSize.
* - SysCallback
* SysCallback allows for user-defined implementations for System APIs.
* The SysCallback support proxy has a smaller code footprint and can be
* used to supply custom System_printf services.
* The default SysCallback functions point to stub functions. See the
* SysCallback module's documentation.
*/
var SysMin = xdc.useModule('xdc.runtime.SysMin');
SysMin.bufSize = 128;
System.SupportProxy = SysMin;
/* ================ Text configuration ================ */
var Text = xdc.useModule('xdc.runtime.Text');
/*
* These strings are placed in the .const section. Setting this parameter to
* false will save space in the .const section. Error, Assert and Log messages
* will print raw ids and args instead of a formatted message.
*
* Pick one:
* - true (default)
* This option loads test string into the .const for easier debugging.
* - false
* This option reduces the .const footprint.
*/
Text.isLoaded = true;
//Text.isLoaded = false;
/* ================ Types configuration ================ */
var Types = xdc.useModule('xdc.runtime.Types');
/*
* This module defines basic constants and types used throughout the
* xdc.runtime package.
*/
/* ================ TI-RTOS middleware configuration ================ */
var mwConfig = xdc.useModule('ti.mw.Config');
/*
* Include TI-RTOS middleware libraries
*/
/* ================ TI-RTOS drivers' configuration ================ */
var driversConfig = xdc.useModule('ti.drivers.Config');
/*
* Include TI-RTOS drivers
*
* Pick one:
* - driversConfig.LibType_NonInstrumented (default)
* Use TI-RTOS drivers library optimized for footprint and performance
* without asserts or logs.
* - driversConfig.LibType_Instrumented
* Use TI-RTOS drivers library for debugging with asserts and logs enabled.
*/
driversConfig.libType = driversConfig.LibType_NonInstrumented;
//driversConfig.libType = driversConfig.LibType_Instrumented;
/* ================ Application Specific Instances ================ */
/* ================ NDK configuration ================ */
var Ndk = xdc.loadPackage('ti.ndk.config');
var Global = xdc.useModule('ti.ndk.config.Global');
var Ip = xdc.useModule('ti.ndk.config.Ip');
var Udp = xdc.useModule('ti.ndk.config.Udp');
var Tcp = xdc.useModule('ti.ndk.config.Tcp');
Global.IPv6 = false;
Global.stackLibType = Global.MIN;
Global.networkOpenHook = "&functionNetworkOpenHook"//"&netOpenHook";
/* automatically call fdOpen/CloseSession for our sockets Task */
Global.autoOpenCloseFD = true;
Global.pktNumFrameBufs = 10;
Global.memRawPageCount = 6;
Global.ndkThreadStackSize = 1536;
Global.lowTaskStackSize = 1024;
Global.normTaskStackSize = 1024;
Global.highTaskStackSize = 1024;
Tcp.transmitBufSize = 1024;
Tcp.receiveBufSize = 1024;
Defaults.common$.diags_ENTRY = xdc.module("xdc.runtime.Diags").RUNTIME_ON;
Ip.ResolveIP = false;
Ip.dhcpClientMode = 1;
Ip.autoIp = false;
Ip.address = "10.7.55.86";
Ip.enableForwarding = false;
Defaults.common$.diags_ENTRY = xdc.module("xdc.runtime.Diags").RUNTIME_ON;
Ip.mask = "255.255.255.0";
Ip.socketIoTimeout = 1;
Ip.domainName = "dcu.net";
Ip.socketConnectTimeout = 5;
Defaults.common$.diags_EXIT = xdc.module("xdc.runtime.Diags").RUNTIME_OFF;
Defaults.common$.diags_STATUS = xdc.module("xdc.runtime.Diags").ALWAYS_OFF;
Ip.routeKeepAliveTime = 1200;
Ip.routeCloneTimeout = 5;
Global.ndkTickPeriod = 1;