Part Number: TMS570LS0714
How / best way to setup MIBSPI so that only first group is HW triggered, and others ARE ONLY triggered after the first has completed transmit & receive?
What I want :
tick --> triggers TG0 --> completes RX and ONLY then, which AUTOMATICALLY triggers next group (TG1), which .. next (TGn).. etc.
What I have now is, EVERY group triggered on rising tick, which then triggers all of them, and , as I understand and see data, it goes by priority or group 0 to N.
Is this the only way to setup what I want, i.e, you have to set same trigger on each? One problem with this is that higher priority group will always supersede others, so if tick happens before my group list completes, it will start back from group 0, which is Not what I want. You can lock group transmit, but this only helps while within One group transmitting.
And i do not want to software /manually trigger next group inside ISR. Just want to make sure I'm not missing some obvious bit setting which allows to do this : TG0 completed -> trigger TG -> next .. next next.