Part Number: TM4C123GH6PZ
Hi TI,
I am designing a board with CAN communication based on the TM4C123GH6PZI.
Attached is the wiring diagram.
Questions:
1-) Is the JTAG connection to connector P1 correct?
2-) Can I use in P1 a 5x2 connector with pitch 1.27 mm (FTSH-105-01-L-DV-K) to debug with the XDS200?
3-) In this case do I need adapters (check image below)?
4-)How can I connect the XDS200 debugger directly to the board without adapters (check image below)?
5-) Do you see any problem in electrical design (power suppy, gnd, ...)?
6-) Is it possible to debug the TM4C123GH6PZI with an XDS100?
Sincerely, Thank you very much. Best Regards.