Part Number: TMDSEMU200-U
Other Parts Discussed in Thread: UNIFLASH
Hi,
My customer uses three TMDSEMU200-U connected to the same PC to production program CC2652.
From the Uniflash CLI they invoke programming with the command dslite -c Config[x].ccxml -e [sw name].hex (x=0, 1 or 2 depending which programmer to start).
This works if the programmers are invoked with a 4 seconds or more delay in between. Shorter delays, or no delay, causes issues and errors like ”no connection to XDS programmer”.
Is there a proper way to launch DSLITE in concurrent sessions on the same PC without the need for delays? The 8 seconds (4+4) extra delay in production programming is highly undesired.
Thanks and regards,
/ Wolfgang