Part Number: TMS570LS3137
Hi,
I am developing on TMDS570LS31HDK using IAR Embedded Workbench for ARM. I read the pwm with the "capGetSignal" command over the HET1[04] pin in HDK and get the frequency.
While reading a frequency value of 74.2 kHz from the same pin with an oscilloscope, capGetSignal returns 78.5 kHz when I examine it with debug.
What is the reason for this frequency difference? I am also sharing the Halcogen configurations that I have made below.
Software;
hetSIGNAL_t signalM;
float64 signalFrequency = 0.0F;
while(true)
{
capGetSignal(hetRAM1, cap2, &signalM);
signalFrequency = 1 / signalM.period;
}