Part Number: TMS570LS1224
Other Parts Discussed in Thread: HALCOGEN,
Hi,
I have enabled RTI and EPWM for ADC notification in the halcogen configuration. I can see the RTI Interupt being triggered in the RTI notification function ,but I cannot see the ADC notification is triggered by the EPWM event. We are trying with no RTOS option.
I am trying to read the ADC value in ADC notification.
following is the code init and while loop.
-
_enable_IRQ();
_enable_interrupt_();
/* Setup ADCs */
adcStartConversion(adcREG1, adcGROUP1);
adcStartConversion(adcREG2, adcGROUP1);
// adcStartConversion(adcREG1, adcGROUP2);
kickerReg->KICKER0 = 0x83E70B13U;
kickerReg->KICKER1 = 0x95A4F1E0U;
pinMuxReg->PINMMR35 = 0x0000;
kickerReg->KICKER0 = 0x00000000U;
kickerReg->KICKER1 = 0x00000000U;
/* setup etPWM */
etpwmSetCount(etpwmREG1, 1000);
etpwmSetCount(etpwmREG2,500);
etpwmSetCount(etpwmREG3, 300);
etpwmSetCounterMode(etpwmREG1, CounterMode_UpDown);
etpwmSetCounterMode(etpwmREG2, CounterMode_UpDown);
etpwmSetCounterMode(etpwmREG3, CounterMode_UpDown);
etpwmSetSyncOut(etpwmREG1,SyncOut_CtrEqZero);
etpwmSetSyncOut(etpwmREG2,SyncOut_EPWMxSYNCI);
etpwmSetSyncOut(etpwmREG3,SyncOut_EPWMxSYNCI);
etpwmREG2->TBCTL |= (uint16)2U << 1U; // PHSEN
etpwmREG3->TBCTL |= (uint16)2U << 1U;
/* Configure mthe module to set PWMA value as 1 when CTR=0 and as 0 when CTR=CmpA */
etpwmActionQualConfig_t configPWM;
configPWM.CtrEqPeriod_Action = ActionQual_Disabled;
configPWM.CtrEqZero_Action = ActionQual_Disabled;
configPWM.CtrEqCmpAUp_Action = ActionQual_Set;
configPWM.CtrEqCmpADown_Action = ActionQual_Clear;
configPWM.CtrEqCmpBUp_Action = ActionQual_Disabled;
configPWM.CtrEqCmpBDown_Action = ActionQual_Disabled;
etpwmSetActionQualPwmA(etpwmREG1, configPWM);
etpwmSetActionQualPwmA(etpwmREG2, configPWM);
etpwmSetActionQualPwmA(etpwmREG3, configPWM);
/* Enable trigger for SOC */
// etpwmEnableSOCA(etpwmREG1, CTR_PRD, EventPeriod_FirstEvent);
//etpwmEnableSOCA(etpwmREG2, CTR_ZERO, EventPeriod_FirstEvent);
etpwmEnableSOCA(etpwmREG1, CTR_PRD, EventPeriod_FirstEvent);
// etpwmClearEventFlag(etpwmREG1, Event_SOCA);
etpwmClearEventFlag(etpwmREG2, Event_SOCA);
// etpwmTriggerEvent(etpwmREG1,Event_SOCA);
etpwmTriggerEvent(etpwmREG2,Event_SOCA);
etpwmDisableCounterLoadOnSync(etpwmREG1);
etpwmEnableCounterLoadOnSync(etpwmREG2, 0, 0x2000);
etpwmEnableCounterLoadOnSync(etpwmREG3, 0, 0x2000);
etpwmEnableTimebasePeriodShadowMode(etpwmREG1);
etpwmEnableTimebasePeriodShadowMode(etpwmREG2);
etpwmEnableTimebasePeriodShadowMode(etpwmREG3);
etpwmEnableCmpAShadowMode(etpwmREG1, LoadMode_CtrEqZero);
etpwmEnableCmpAShadowMode(etpwmREG2, LoadMode_CtrEqZero);
etpwmEnableCmpAShadowMode(etpwmREG3, LoadMode_CtrEqZero);
etpwmDeadBandConfig_t deadbandconfig;
deadbandconfig.halfCycleEnable = true;
deadbandconfig.inputmode = PWMA_RED_FED;
deadbandconfig.outputmode = PWMB_FED_PWMA_RED;
deadbandconfig.polarity = Invert_PWMB;
etpwmSetDeadBandDelay(etpwmREG1,112,112);
etpwmSetDeadBandDelay(etpwmREG2,112,112);
etpwmSetDeadBandDelay(etpwmREG3,112,112);
etpwmEnableDeadBand(etpwmREG1, deadbandconfig);
etpwmEnableDeadBand(etpwmREG2, deadbandconfig);
etpwmEnableDeadBand(etpwmREG3, deadbandconfig);
// rti config
rtiCOMPARE2_PER = rtiGetPeriod(rtiCOMPARE2);
rtiCOMPARE1_PER_NEW = rtiGetPeriod(rtiCOMPARE1);
/* Start RTI Counter Block 0 */
// rtiStartCounter(rtiCOUNTER_BLOCK0);etpwmStartTBCLK();
adcEnableNotification(adcREG1, adcGROUP1);
adcEnableNotification(adcREG2, adcGROUP1);
adcStartConversion(adcREG1, adcGROUP1);
adcStartConversion(adcREG2, adcGROUP1);
rtiEnableNotification(rtiNOTIFICATION_COMPARE0);while(1)
{//user code
}