Part Number: EK-TM4C123GXL
Other Parts Discussed in Thread: UNIFLASH,
Hello,
customer wants to use the emulator on the launchpad to debug their application. What emulator has he to configure in CCS or Uniflash? XDS100v2?
Regards, Holger
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: EK-TM4C123GXL
Other Parts Discussed in Thread: UNIFLASH,
Hello,
customer wants to use the emulator on the launchpad to debug their application. What emulator has he to configure in CCS or Uniflash? XDS100v2?
Regards, Holger
Hi,
The on-board debug probe is called ICDI. In CCS, you need to specify Stellaris In-Circuit Debug Interface.
If you want to use the debug probe on the EK-TM4C123GXL to debug out another board, use this app note for reference in section 4.6.
Hello Charles,
is it possible to use the EK-TM4C123GXL to debug another MCU like C2000? If yes what emulator do I have to use in CCS? XDS100v2?
Regards, Holger
HI Holger,
I thought I already answered the question. The emulator to specify is ICDI (Stellaris In-Circuit Debug Interface) in CCS.
is it possible to use the EK-TM4C123GXL to debug another MCU like C2000? I
The Stellaris In-Circuit Debug Interface (IDCI) on the EK-TM4C123GXL only supports microcontrollers with a Cortex-M3 or Cortex-M4 CPU, so C2000 MCU's aren't supported.
If you open the Target Configuration editor in CCS, and select Stellaris In-Circuit Interface as the Connection, then you can see the supported devices: