Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C1290NCPDT: Replace with TM4C129ENCPDTI3R

Part Number: TM4C1290NCPDT
Other Parts Discussed in Thread: TM4C129ENCPDT

Our customer's original design used these two ICs. I preliminarily compared them. Now, tm4c129encpdti3r has some more functions, and the pins are compatible. Please confirm whether tm4c129encpdti3r can directly replace tm4c1290ncpdti3r without changing the original PCB and program?

  • HI,

      See the difference between the two. TM4C129ENCPDT has Ethernet. Some Ethernet pins are dedicated pins. They can not be repurposed as GPIO pins as in TM4C1290NCPDT. TM4C129ENCPDT cannot be used as a replacement. 

    TM4C1290NCPDT

    TM4C129ENCPDT

    TI.com inventory 0 0
    CPU Arm Cortex-M4F Arm Cortex-M4F
    Frequency (MHz) 120 120
    Flash memory (KB) 1024 1024
    RAM (KB) 256 256
    ADC 12-bit SAR 12-bit SAR
    GPIO 90 90
    UART 8 8
    Number of I2Cs 10 10
    Package Group
    TQFP | 128
    TQFP | 128
    Features
    Hibernation with calendar mode
    8-/16-/32-bit EPI
    Hibernation with calendar mode
    Hardware encrpytion (AES/DES/SHA/MD5)
    8-/16-/32-bit EPI
    Approx. price (USD)
    $5.490 | 1ku
    $7.000 | 1ku
    Ethernet No Yes
    PWM (Ch) 8 8
    SPI 4 4
    USB Yes Yes
    CAN (#) 2 2
    Communication interface
    CAN
    I2C
    SSI/SPI
    UART
    USB 2.0 OTG/host/device
    10/100 Ethernet MAC+PHY
    CAN
    I2C
    SSI/SPI
    UART
    USB 2.0 OTG/host/device