This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCU reference for a specific automotive application

Hi

For an automotive application, I am looking for an MCU with the characteristics below:

-8 input capture (for frequency and duty cycle measurement of 8 external signals)
-8 PWM outputs
-8 ADC inputs (or an external model with the same number of ADC inputs and which can be communicated in SPI)
-CAN communication
-SPI communication

Can you help me to find the right MCU reference?

Thank you 

  • Hi,

      If you are looking for AEC-Q100 and functional safety compliant MCU for automotive applications, please look at TMS570LS or RM MCUs as they meet your itemized requirements. 

      If  AEC-Q100 and functional safety compliant are not required then there are more options. You can also consider TM4C123 and TM4C129 MCUs. Both MCUs will meet your functional requirements but with different on-chip memory and performance offerings.