Part Number: TMS570LS3137
Hi,
I'd like to have secondary bootloader on Bank1 to update main bootloader on Bank0.
Also i have the application on bank1.
I am on CCS9.3
Linker commad file is like below:
MEMORY
{
BOOTVECTORS (X) : origin=0x00000000 length=0x00000020
BOOTFLASH (RX) : origin=0x00000020 length=0x0007FFE0
BOOT1VECTORS (RX) : origin=0x00180000 length=0x00180020
BOOT1FLASH (RX) : origin=0x00180020 length=0x0003FFE0
APPVECTORS (RX) : origin=0x001C0000 length=0x00000020
APPFLASH (RX) : origin=0x001C0020 length=0x0013FFC0
APPINFO (RX) : origin=0x002FFFE0 length=0x00000020
STACKS (RW) : origin=0x08000000 length=0x00001500
RAM (RW) : origin=0x08001500 length=0x0003EB00
}
SECTIONS
{
.intvecs : {} > BOOTVECTORS
.text : {} > BOOTFLASH
.const : {} > BOOTFLASH
.cinit : {} > BOOTFLASH
.pinit : {} > BOOTFLASH
.bss : {} > RAM
.data : {} > RAM
.sysmem : {} > RAM
}
When i try to compile , i get memory range overlap errors like below:
#10010 errors encountered during linking; "BootloaderPGEClipped_JumpBL2.out" not built
#10264 APPFLASH memory range overlaps existing memory range BOOT1VECTORS
#10264 APPINFO memory range overlaps existing memory range BOOT1VECTORS
#10264 APPVECTORS memory range overlaps existing memory range BOOT1VECTORS
#10264 BOOT1FLASH memory range overlaps existing memory range BOOT1VECTORS
gmake: *** [all] Error 2
gmake[1]: *** [BootloaderPGEClipped_JumpBL2.out] Error 1
gmake[1]: Target 'secondary-outputs' not remade because of errors.
Thanks in advance.