Part Number: TMS570LS3137
Hi experts,
My customer is testing the time of the SPI Slave Td(scsl-senal)s.
The time of Td(scsl-senal)s is as follows of DS.(CSHOLD = 0, CLOCK PHASE = 0, clock polarity = 0)

The formula for calculating the MAX value is as follows.
tc(vclk)+Tf(enan)s[ena]+27
The customer parameters are as follows.
| Parameter | Item | Parameter | unit |
| f(vclk) | 90 | MHz | |
| tc(vclk) | 11.11111111 | ns | |
| Tc(spc)m [clock] |
66.592 | ns | |
| Tr(spc)m[clock] | 2.5 | ns | |
| Tf(spc)m[clock] | 2.5 | ns | |
| Tr(spics)m[cs] | 2.5 | ns | |
| Tf(spics)m[cs] | 2.5 | ns | |
| Tr(miso)m[miso] | 2.5 | ns | |
| Tr(enan)s[ena] | 17.40 | ns | |
| Tf(enan)s[ena] | 3.72 | ns | |
| C2Tdelay | 8 | - | |
| T2Cdelay | 8 | - |
Calculating Td(scsl-senal)s using this parameter the following:
=tc(vclk)+Tf(enan)s[ena]+27
=11.11 + 3.72 + 27
= 41.83ns
However, when the customer measures this waveform on the customer's original board, this value is 87.56ns.
In other words, it exceeds the maximum value of DS.
Do you know why this value exceeds the maximum value for DS?
Other than this parameter, it is within the range of the maximum value, so the waveform is correct except for this parameter.
The customers use two TMS570LS3137 boards, one for the SPI master and the other for the SPI slave for communication.
Best regards,
Sasaki