Part Number: TMS570LS0914
The documentation states that there are 8 GIOA's and 8 GIOB's. I can find 8 GIOA's but only 4 GIOB's (0-3)?
On which pins are the last 4 GIOB's (4-7) located?
I'm working with the PGE housing.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LS0914
The documentation states that there are 8 GIOA's and 8 GIOB's. I can find 8 GIOA's but only 4 GIOB's (0-3)?
On which pins are the last 4 GIOB's (4-7) located?
I'm working with the PGE housing.
What about the statement (see below) in the datasheet which suggests that I can use all or some of the N2HET pins as GIO's?
N2HET can be used for pulse-width-modulated outputs,
capture or compare inputs, or general-purpose I/O (GIO).
All other the 16 GIO signals are supported by LS0915 PGE package
Sorry for typo. Not all 16 GIO signals are supported by LS0914 package. There is no LS0915.
What about the statement (see below) in the datasheet which suggests that I can use all or some of the N2HET pins as GIO's?
Yes, you can use all the N2HET pins as GIO pins.